Выполните поиск по ключевым словам, коду изделия, коду заказа или серийному номеру, например: «CM442» или «Техническое описание»
Для начала поиска введите минимум 2 символа.
  • История

Endress+Hauser wins Hermes Award

Hannover Messe recognizes the world’s first self-calibrating thermometer: iTHERM TrustSens

Дата публикации: 23.04.2018

The compact thermometer iTHERM TrustSens has been designed especially for hygienic and aseptic applications in the food & beverage and life sciences industries. With automated and fully traceable self-calibration during production, the sensor eliminates the risk of undetected non-conformities, resulting in maximum product safety and process efficiency. The integrated Heartbeat Technology additionally allows for continuous device diagnostics and verification without interruption of the process.

Developers used physics phenomenon

iTHERM TrustSens relies on an integrated reference sensor. The developers used the so-called Curie point physics principle, in which the magnetic properties of a material abruptly change at a specific temperature point. This point is determined for the reference sensor.

As soon as the temperature falls below this value, following a steam sterilization for example, the primary sensor calibrates itself against the reference. Since the Curie point remains constant, the reference sensor as a master provides a stable comparison value.

The probe thus calibrates itself each time the system is cleaned or sterilized as is usual in processes in the food & beverage and life science industries. The added value for customers is huge. Large systems often include hundreds of temperature sensors that have to be calibrated several times a year. To date, this has required stopping the process and removing the instruments. iTHERM TrustSens omits that.

Sensor technology for the IIoT

“The award-winning product makes a major contribution to the deployment of the Industrial Internet of Things throughout the process industry,” said Jochen Köckler, CEO of Deutsche Messe. The award was presented at the opening of Hannover Messe 2018 in front of many guests, among them Germany’s Chancellor Angela Merkel. The Hermes Award is one of the most respected technology contests worldwide and recognizes products and processes characterized by innovation, efficiency and application benefits.

iTHERM TrustSens will be on show at Hannover Messe 2018 (23–27 April 2018) at the Endress+Hauser booth (hall 11, booth C43).

View our video about the iTHERM TrustSens technology on YouTube.

Загрузки

    EH_2018-04-23_Hermes_Award_for_TrustSens.zip

База пресс-релизов

Подпишитесь на рассылку Endress+Hauser, чтобы быть в курсе последних новостей компании.

Новостная рассылка Endress+Hauser

Подписка на новостную рассылку Endress+Hauser позволит всегда оставаться в курсе последних событий компании, получать актуальные новости и полезные статьи.

Выберите интересующие вас темы: *
Выберите интересующие вас отрасли:

Личные данные

Поля, отмеченные *, являются обязательными для заполнения. Вы получите электронное письмо с подтверждением подписки и соответствующей ссылкой. Ваши данные будут использованы только для персонализации вашей рассылки и не будут переданы третьим лицам. Информация вносится добровольно. Мы будем осуществлять анонимное отслеживание ссылок для сбора статистических данных.

Контакты

Добро пожаловать на сайт компании Endress+Hauser!

Выберите рынок / регион