Industrial Ethernet Training PROFINET

A hands-on based course, recognized in all industries

By becoming familiar with the PROFINET protocol you will learn about the advantages of PROFINET technology as well as procedures for troubleshooting.
At the end of the course you will be able to plan a PROFINET system and bring it into operation. The course focuses on the link between PROFINET and PROFIBUS PA as well as HART.

Содержание

  • In the theoretical part the following content is covered:
    ISO/OSI model, types of wires and components, network structures and network calculations and
    grounding and shielding concepts.

  • Drivers, name assignment and addressing, commissioning procedures and troubleshooting procedures.

  • In the practical part the following content is covered:
    Wiring of PROFINET networks, device setup, commissioning of an own PROFNET network, troubleshooting a PROFINET network.

Задачи

  • At the end of the course you will understand PROFINET networks in an industrial environment. You will learn about the benefits of PROFINET technology in industrial applications, but also about possible outside influences.

Кому это будет интересно?

  • Technicians/Maintenance Technicians

  • Service/Support Specialists

  • Supervisors

  • Programmers/Device Configurators

  • Engineers

Предварительные условия

Basic knowledge of electronics and ability to use a computer.

Квалификация

The training is Endress+Hauser certified.

Метод оценки

Participants are given time to work with the various components of a PROFINET network.

We put emphasis on a balanced approach to theory and practice as well as a vendor-neutral atmosphere.

Mornings are spent learning the theoretical background and afternoons with the actual components and integration of the field devices into the system.
Almost half the course is spent on giving you ample opportunity to use what you have learned in hands-on tasks taken straight from our experience.

Тип

A hands-on based course, recognized in all industries.

Контакты

Выберите рынок / регион