How can improved thickener performance support safer tailings management?
Improve tailings management through stable thickener performance, reliable water recovery and better process visibility
In brief
- Stable thickener performance supports safer tailings management by maintaining more consistent underflow conditions for downstream transport and deposition.
- Consistent underflow density improves water recovery, helping reduce freshwater demand while keeping tailings suitable for pumping and handling.
- Reliable process visibility helps operators respond to changing ore and slurry conditions, using a range of measured values to maintain process stability.
- Integrated monitoring reduces operational risk and supports plant continuity by helping teams identify deviations early and avoid thickener, pipeline and tailings facility bottlenecks.
A lifecycle approach to tailings management
Effective tailings management starts upstream, in the processing plant. Thickener performance determines how much water is recovered and how stable the tailings are when they reach downstream tailings systems, such as Tailings Storage Facilities (TSF).
The Global Industry Standard on Tailings Management treats tailings as a lifecycle responsibility, from planning and design through operation, monitoring and closure. Thickening and dewatering are key to water recovery and influence the rheology of the tailings sent downstream.
Ore coming into the plant and slurry conditions change inside the process plant can change constantly. Particle size and distribution, settling time, viscosity, solids composition, rheology etc can all affect the tailings settling behaviour . Process visibility gives operators the information to respond to these changes and keep mine tailings properties within a safe operating range.
Why is thickener performance critical for safe tailings management?
Thickener performance sets the water content and consistency of the tailings sent downstream. Fluctuations in underflow solids concentration and flow rate affect both tailings transport and deposition.
Changes in underflow solids concentration and flow rate can affect tailings transport and deposition. In an analysis of operating data from four mines, predicted beach slopes for four conditions at one gold operation ranged from 1.6% to 3.1% as the recorded underflow solids concentration varied from 52.3% to 64.3%. The study demonstrates why thickener-performance variability should be considered when designing and operating tailings transport and storage systems.
The thickening and dewatering processes are critical for the plant water balance. Recovering water before disposal reduces slurry volumes and returns water to the process, reducing energy consumption. The operating challenge is to maximize water recovery while keeping the underflow suitable for pumping and deposition.
How can stable underflow density improve water recovery?
Stable underflow density keeps dewatering consistent, so more water is reliably separated and returned to the process. It also gives tailings transport systems predictable material to handle. One study has shown through operating data from four mines that actual thickener performance can differ significantly from design assumptions. Downstream systems designed for one set of conditions may receive something quite different in daily operation. This can make it quite difficult to control a process, and as a result, many operators err on the side of caution and run tailings underflow setpoints conservatively to avoid the likelihood of equipment damage or blockages of the tailings disposal systems.
The right density target for the tailings disposal line depends on slurry behaviour. CSIRO notes that finer grinds, higher solids concentrations and higher clay contents make slurries more complex, with direct effects on thickener performance, pipeline transport and deposition. Two slurries with the same density can flow very differently.
As a result, density data is most valuable when read together with information on slurry characteristics. This combination lets process engineers push water recovery without creating transport problems downstream.
How to maintain stable thickener performance?
Stable operation depends on seeing feed and slurry changes early and adjusting before they affect underflow quality. Ore variability shifts particle size, mineralogy, clay content and solids concentration, and each of these changes settling behaviour.
Fine particles are a common source of instability. CSIRO testing found large differences in settling flux between particle size distributions produced from the same iron ore. Poor flocculation can also limit throughput or produce underflow with unfavourable properties.
Stable operation depends on seeing feed and slurry changes early and adjusting before they affect underflow quality. Ore variability shifts particle size, mineralogy, clay content and solids concentration, and each of these changes settling behaviour.
Fine particles are a common source of instability. CSIRO testing found large differences in settling flux between particle size distributions produced from the same iron ore. Poor flocculation can also limit throughput or produce underflow with unfavourable properties.
Thickener interface tracking methods for process visibility
Bed level and interface measurements provide the most direct view of what is happening inside the thickener. Combined with slurry density measurement, flow, bed mass, thickener overflow clarity and rake torque data, they show changes in solids inventory and settling conditions before those changes appear in the underflow.
Selection of technology for measuring the thickener interface depends on the thickener design, feed rate and slurry properties. Buildup, turbulence or a diffuse interface can all affect measurement performance, so the technology must suit the specific application.
From non-contact measurement technologies such as ultrasonic (and now such sensors can deliver information such as sedimentation factor), to mechanical divers to measure a level, to more technologically advanced mechanical diver solutions to deliver thickener density profiling, there are many reliable options available depending on the factors mentioned above.
How can you reduce operational and environmental risks across the tailings process?
Operational and environmental risks are reduced through coordinated engineering, monitoring and governance across the full tailings’ lifecycle. Process visibility in the plant contributes by giving every team reliable information about the tailings entering downstream systems.
The ICMM Tailings Management Good Practice Guide links governance and engineering practices across the facility lifecycle. Thickener data fits into this framework as an upstream source of operational evidence.
Better upstream data reduces uncertainty, but comprehensive downstream monitoring can also bring insights beyond the regulatory requirements. Measuring parameters such as soil moisture, groundwater level and quality, discharge water quality and surface dam levels can all help manage the entire tailings system more effectively.
How real-time tailings monitoring support safer operations
Continuous measurement shortens the time between a change occurring and the team responding to it. Early detection allows deviations to be investigated and managed under established site procedures.
Plant data and facility monitoring answer different questions. Thickener measurements describe the material being delivered, while facility monitoring tracks indicators such as water levels and pore pressure. Connecting both gives engineers the context to judge which changes require action.
How sustainable mine water management cuts operating costs
Recovering water at the thickener reduces the volume of fresh water a plant needs and lowers the volume of water sent to the tailings facility. Savings depend on local water availability, pumping distances, treatment needs and energy costs. Where freshwater supply, pumping or treatment carries significant cost, improved water recovery can also help reduce operating expenditure.
Stable thickener performance makes recovered water supply more predictable for the processing circuit. This strengthens both the site water balance and its environmental performance.
How can effective tailings management protect plant performance and continuity?
Effective tailings management keeps water shortages and waste transportation routes from turning into production constraints, affecting plant utilisation. Stable thickener performance helps maintain consistent operating conditions across the processing plant.
One of the largest risks that would keep a Processing Plant Manager up at night is that the thickener has bogged or the tailings line has blocked. The downtime from incidents such as these can lead into several days, just to clear the blockage and clean the thickener. Downtime increases if the thickener is a confined space or hard to access for cleaning crews. Continuous visibility lets engineers see when the process approaches downstream limits and adjust before downtime occurs.
Shared process data also aligns process engineers, instrumentation specialists, water teams and tailings facility managers around one operating picture. Decisions reflect the whole system, which strengthens operational resilience and production continuity.
Successful tailings management begins with stable thickener performance. Consistent underflow and reliable water recovery give downstream systems the conditions they were designed for .Process visibility via sufficient and reliable instrumentation makes that stability achievable as ore conditions change. Density, flow, interface and rheology data each answer a specific operating question. Combined with sound engineering and governance across the tailings lifecycle, better upstream visibility supports operational efficiency, risk reduction and long-term sustainability.
Frequently asked questions about thickener performance and tailings management
This section answers common questions about thickener performance, tailings management and process monitoring. It explains how stable underflow density, reliable instrumentation and improved process visibility can support water recovery, operational stability and safer tailings operations.