Reliable compliance with limit values
Demand-oriented dosing saves up to 40% of flocculant
Together with Endress+Hauser, Veolia Wasser Deutschland GmbH has developed a solution for the demand-oriented and automated flocculant dosing in the aeration basins of the wastewater treatment plant in Colditz.
Results
-
Reliable compliance with legal limits for orthophosphate
-
Precise dosing of the flocculant according to requirements
-
Reduced operating costs
-
Increased operational reliability through remote access
-
Fast response times in case of disruption
Customer challenge
Compliance with legally prescribed limit values for orthophosphate posed a number of challenges for the wastewater treatment plant in Colditz. Previously, the flocculant was dosed on the basis of weekly laboratory analyses – however, these only provided selective results and were unable to record fluctuations depending on the time of day or week. Continuous and more precise monitoring of the phosphate content was necessary in order to meet the increasing requirements in the long term.
Our solutions
Endress+Hauser partnered with Veolia to implement continuous phosphate monitoring using the CA80PH analyzer. It measures phosphate levels in two aeration basins, enabling precise dosing of flocculant.
Digital technologies were also used: The measurement data is transmitted in real time via the Netilion Cloud. This allows maintenance requirements to be recognized immediately. Thanks to additional remote access, the Endress+Hauser service team can access the analyzer directly.